Get | /projects/{projectId} returns the project name for the given project id |
Get | /projects/{projectId}/classes returns the list of classes in a project |
Get | /projects/{projectId}/devices returns an array of devices in the project optionally filtered by port prefix |
Get | /projects/{projectId}/historianConnections returns a list of historianConnections in a project that satisfy the filter criteria |
Post | /projects/{projectId}/historianConnections Creates or updates an array of historian connections in the project |
Post | /Projects/{projectId}/historianConnections:batchDelete Deletes an array of historain connections in the project |
Post | /projects/{projectId}/historianConnections:read Gets an array of historian connection objects that satisfy the filter criteria specified in the request body. |
Get | /projects/{projectId}/objects returns a list of objects in a project that satisfy the filter criteria |
Post | /projects/{projectId}/objects Creates or updates an array of objects in the project |
Post | /Projects/{projectId}/objects:batchDelete Deletes an array of objects in the project |
Post | /projects/{projectId}/objects:read Gets an array of class Objects that satisfy the filter criteria specified in the request body. |
Post | /projects/{projectId}/operationsHub-settings Add or individually modify parameters related to Operations Hub |
Get | /projects/{projectId}/points Gets an array of point objects that satisfy the query criteria |
Post | /projects/{projectId}/points Creates or updates an array of points in the project |
Post | /Projects/{projectId}/points:batchDelete Deletes an array of points in the project |
Post | /projects/{projectId}/points:read Gets an array of point objects that satisfy the filter criteria specified in the request body. |
Get | /projects/{projectId}/resources returns a list of resources in a project that satisfy the filter criteria |
Post | /projects/{projectId}/resources Creates or updates an array of resources in the project |
Post | /Projects/{projectId}/resources:batchDelete Deletes an array of resources in the project |
Post | /projects/{projectId}/resources:read Gets an array of resource objects that satisfy the filter criteria specified in the request body. |
Get | /projects/{projectId}/roles returns a list of roles in a project that satisfy the filter criteria |
Post | /projects/{projectId}/roles Creates or updates an array of roles in the project |
Post | /Projects/{projectId}/roles:batchDelete Deletes an array of roles in the project |
Post | /projects/{projectId}/roles:read Gets an array of role objects that satisfy the filter criteria specified in the request body. |
Get | /Projects/{projectId}/runningStatus returns a running status of the CIMPLICITY project |
Post | /Projects/{projectId}/runningStatus start or stop a CIMPLICITY project |
Post | /Projects/{projectId}/runningStatus:read Deletes an array of objects in the project |
Get | /projects/{projectId}/SQLConnections Gets an array of SQL connections objects that satisfy the query criteria |
Post | /projects/{projectId}/SQLConnections Creates or updates an array of sql connections in the project |
Post | /projects/{projectId}/SQLConnections:read Gets an array of SQL Connections that satisfy the filter criteria specified in the request body. |
Get | /projects/{projectId}/users returns a list of users in a project that satisfy the filter criteria |
Post | /projects/{projectId}/users Creates or updates an array of users in the project |
Post | /Projects/{projectId}/users:batchDelete Deletes an array of users in the project |
Post | /projects/{projectId}/users:read Gets an array of users objects that satisfy the filter criteria specified in the request body. |
Post | /rest-settings modifies rest settings of multiple projects |
Get | /service-settings returns settings that can be used by the client |
Post | /user-config creates or modifies a user |